Feed_Constant (Feed)

Index.Sub 6092.1H
Data Type Unsigned32
Access Read
PDO Mappable RX_DO (1)
Unit User-defined position unit

Range

1 to 4294967295
Default Value 200
Store Supported Yes
Description

This object is used to calculate the ratio of Feed (given in user-defined position units) per Driving Shaft revolutions :

            

Notes

  • This object is available with firmware V00r80 or superior.

  • See Factor Group.

  • (1) available with firmware V03r02 or superior.